PUCCH Common (Advanced LTE-A Pro FDD Uplink)

Additional Uplink parameters are described in Cell Parameters (Advanced LTE-A Pro FDD Uplink), PUSCH Common (Advanced LTE-A Pro FDD Uplink), and Sounding Reference (Advanced LTE-A Pro FDD Uplink). 

PUCCH Common

PUCCH Auto-calculate per-slot parms

N_RB(2)

N_CS(1)

nPUCCH(2,0)

nPUCCH(2,1)

Delta Shift PUCCH

PUCCH Auto-calculate per-slot params

Choice: Off | On

Default Off

To enable manual input for the following parameters, set PUCCH Auto-calculate per-slot params to Off:

Grp Idx for slot 0/1, OS Idx for slot 0/1, Cyclic Shift for slot 0/1, and DMRS CS for slot 0/1in the UCI Tx sequence window.

To enable manual input for the following parameters, set PUCCH Auto-calculate per-slot params to On:

PUCCH_RB(2), PUCCH_CS(1), PUCCH n(1), PUSCH, PUCCH n(2), PUSCH Delta Shift, and PUCCH Delta Offset (described below)

Hopping in the Cell Parameters section of the Uplink node.

Double-click or use the drop-down menu to turn automatic calculation of per-slot parameters on or off.

N_RB(2)

Range: 0 to (Maximum resource blocks - 1)

Default: 0

When PUCCH Auto-calculate per-slot params is turned On, you can set this value. This is one of the values used for generating and mapping PUCCH and DMRS PUCCH (see 3GPP TS36.211).

N_CS(1)

Range: 0 to 7 (integer)

Default: 0

When PUCCH Auto-calculate per-slot params is set to On, you can set this value. This is one of the values used for generating and mapping PUCCH and DMRS PUCCH (see 3GPP TS36.211).

nPUCCH (2,0)

Range: 0 to Calculated Value

Note: The Calculated Value depends on the PUCCH settings.

Default: 0

Enter the PUCCH format 2/2a/2b resource index nPUCCH(2,0) for antenna port P0.

This parameter is active, when the PUCCH Auto-calculate per-slot params is On. Otherwise it’s read only.

When PUCCH Auto-calculate per-slot params is set to Off, this value is read only.

The calculated value specifies the number of resource blocks for the PUCCH formats 2/2a/2b.

Calculated Value:

Default: 0

Refer to 3GPP TS36.211, 36.212 and 36.213.

nPUCCH (2,1)

Range: 0 to Calculated Value

Note: The Calculated Value depends on the PUCCH settings.

Default: 0

Enter the PUCCH format 2/2a/2b resource index nPUCCH(2,1) for antenna port P1.

This parameter is active, when the PUCCH Auto-calculate per-slot params is On. Otherwise it’s read only.

When PUCCH Auto-calculate per-slot params is set to Off, this value is read only.

The calculated value specifies the number of resource blocks for the PUCCH formats 2/2a/2b.

Calculated Value:

Default: 0

Refer to 3GPP TS36.211, 36.212 and 36.213.

PUCCH Delta Shift

Range: 1 to 3

Default: 1

When PUCCH Auto-calculate per-slot params is turned On, you can set this value. This is one of the values used for generating and mapping PUCCH and DMRS PUCCH (see 3GPP TS36.211).